No compatible emulators available WIN10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No compatible emulators available WIN10

1,922 次查看
ivoisaia
Contributor I

Hi guys,

I have installed LPCXpresso v8.2.2 on my Win10 but when i debug the project this error appears: "No compatible emulators available". The LPC-Link is connected, powered and it is not already in use, I also tried to use LPC-Link2 but it's the sam.

When LPC_link is connect, in Device Manager appear "LPC-Link Probe v1.3" (hardware type: Controller USB).

When I run boot_link1 as described in the link
** Latest version of LPCXpresso IDE : v8.1.4 **
http://www.lpcware.com/content/forum/lpcxpresso-latest-release

It appears this error: "No device connected. Press Download when connected".

Any help will be appreciated

Ivo

0 项奖励
回复
1 回复

1,391 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the below links and let me know if this helps.

Launch Configuration Menu 

Link2 Debugger/Emulator Not Found | www.LPCware.com 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复