No GUI Files Error while creating a library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No GUI Files Error while creating a library

2,040件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mohammadyou on Sat May 30 20:57:52 MST 2015
Hi all.
based on the DOC I want to create a library so I copied the makefile.bat and the others requirements (prep.bat - CC.bat - Lib.bat from 'ARM-IAR' Folder) to the root directory (inside 'start' folder of 'emWin BSP') and Edited the Prep.bat and point it to the folder of IAR Toolpath  I face a problem same as below. before clicking closing the CMD Window the 'Temp' and 'Lib' folder is created but after that it's gone!!
would you please tell me what the problem ?
[img=630x377]http://www.lpcware.com/system/files/1_0.png[/img]
ラベル(1)
0 件の賞賛
返信
0 返答(返信)