No Bulk interrupts LPC54628

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Bulk interrupts LPC54628

Jump to solution
3,285 Views
whinis
Contributor I

I am unsure if I just have something misconfigured or truly just don't understand how it works.

I am using the LPC54628 on the OM13098 board and my goal is to send graphics to the screen using bulk transports on usb1. My plan was to use the composite device example and replace one of the HID classes with a simpler consumer device report with 6 buttons and  and the other with a modified CDC ACM example that would directly draw to the frame buffer. Modifying the HID was no issue and and on both linux and windows I had a 1 byte report that could show the value of buttons pressed. However I have been unable to get the CDC ACM example working in the composite class.

Endpoint setup appears to go fine such that I have 5 endpoints in total not including control. Bulk in/out on endpoint 1, Interrupt In/Out on 2, and Interrupt In for Hid on 3. I see no errors reported on endpoint init however I never get an interrupt for any bulk transfers. To initiate the bulk transfers I am using libusb

libusb_bulk_transfer(
            lcdhandle_,
            endpoint_out_,
            lcd_buffer,
            sizeof(lcd_buffer),
            &len,
            250
            );

 that you can see here. I get a timeout every time without any interrupt even on USB1_IRQHandler.  From what I can see interrupts are enabled on INTEN for all endpoints. Is there some configuration I am missing ?

Labels (3)
0 Kudos
Reply
1 Solution
3,264 Views
belmontbob59
Contributor IV

You should put a USB com analyzer to see the traffic and pinpoint which side the issue is. Either the host request does not come down the wire or the device side's EP is not primed.

View solution in original post

0 Kudos
Reply
2 Replies
3,265 Views
belmontbob59
Contributor IV

You should put a USB com analyzer to see the traffic and pinpoint which side the issue is. Either the host request does not come down the wire or the device side's EP is not primed.

0 Kudos
Reply
3,261 Views
whinis
Contributor I

It ended up being the priming, I didn't realize I needed todo that so while the endpoint was configured it was never primed.

0 Kudos
Reply