Need the library file for lpc2148 for LPCXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need the library file for lpc2148 for LPCXpresso IDE

1,421 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Asim27902 on Sun Dec 28 00:27:28 MST 2014
Hello All,

I'm currently using the free edition of LPCXpresso, I have observed that LPC2148 is not supported with LPCXpresso, since my program size for LPC2148 is smaller than 128KB, I wanted to use LPCXpresso for development with LPC2148. ( It would look something like this ex. CMSISv2p00_LPC2xxx) If any of you can provide me with the file, I would be thankful.
regards,
Asim Sayed
Assistant Professor
AISSMSCOE, Pune
Maharashtra, India
标签 (1)
0 项奖励
回复
1 回复

1,112 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Dec 28 01:25:55 MST 2014
There is no such file.

CMSIS stands for Cortex Microcontroller ... And LPC2000 is not Cortex.

You will find some header files in a zip file called old headers I. The examples directory. But there is no library.
0 项奖励
回复