Content originally posted in LPCWare by Martin84 on Tue May 20 02:35:27 MST 2014
Quote: 
I am using LPC1769. I configured pin P2.10 as GPIO, but when board is connected to the application, code is running strangely and debugging is not possible. When I disconnected pin P2.10 only, everything works fine. I tried repeat connection/disconnection of P2.10 and still with same result (connected=NOK, disconnected=OK). Do you know what can be the reason of such behavior? Pin P2.10 is physically connected to base of the bipolar NPN transistor.
Thank you.
That's exactly the same Problem.
In the attachment there is the problem shown...
I will try it when I'm home. I think I will avoid using the P0.1.
Thank you very much for the great answer :-) I will report the results of this solution!
Regards, Martin