Need help getting started with OM13054 boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help getting started with OM13054 boards

1,464件の閲覧回数
zmrwest
Contributor I

I'm new to NXP LPC's and I am starting a project with 2 OM13054 boards in hand.  I have MCUXpresso installed and I am trying to debug peripheral blink program.  I get a "can't connect error".  I remember reading that I could use one link 2 board to debug the target board but can't find any details on how to do that.  How do I setup to use one 54 board to debug the other?

Also, I'm trying to use the config tool to look at the lpc4370 pins but I can figure out how to do that.

Thanks in advance, Bill

ラベル(1)
0 件の賞賛
返信
1 返信

1,392件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You want to use  OM13054 boards as LPC-Link2 debug tool.  Thus please follow this picture to connect the board:

pastedImage_1.png

For more about LPC-Link2, see LPC-Link2 | NXP 

There are several video on this link which tells how to use it.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信