Need help for IAR EWARM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need help for IAR EWARM

1,276 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andyyau on Sun May 26 10:10:23 MST 2013

Hi,


I am new to LPC and staring IAR EWARM. It is not easy to get information of the following:


1. How to create a brand new project with CMSIS support for LPC1114? I cannot find any code template for it.


2. Where is the LPC1114 peripheral drivers of for ADC, UART, Timer...?


3. I tried LPCopen drivers, but my EWARM versoin is 6.4. When I open the project, it will get error as 6.5.2 is required. Any way to fix this?


Thanks a lot!


Andy

标签 (1)
0 项奖励
回复
1 回复

1,265 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Mon Jun 03 10:05:00 MST 2013

There will be an IAR verison of the project guide (similar to the Xpresso project guide) for the next version of LPCOpen. However, you can get information on needed files, include paths, etc. from the current Xpresso version of the project guide @ http://docs.lpcware.com/lpcopen/v1.03/_l_p_c_o_p_e_n__x_p_r_e_s_s_o__p_r_o_j_e_c_t__p_o_r_t_i_n_g__g...


http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-upcoming-re...

0 项奖励
回复