Need LPC2468 Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need LPC2468 Drivers

1,302 Views
Nandini_19
Contributor I
Does LPC24xx(LPC2468) controller has Device drivers???? Regards, Nandini
0 Kudos
Reply
1 Reply

1,288 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Nandini,

You can find examples and drivers for this device in the Embedded Software section of this link:

Single-chip 16-bit/32-bit micro; 512 kB flash, Ethernet, CAN, ISP/IAP, USB 2.0 device/host/OTG, exte... 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.------------------------------------------------------------------------------ 

0 Kudos
Reply