Need Help: Initalize IS42S16400J on LPC4357, M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Help: Initalize IS42S16400J on LPC4357, M4

1,222 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alastair on Tue Jun 23 02:17:24 MST 2015
Hi
I want to use SDRAM  IS42S16400J(1 Meg Bits x 16 Bits x 4 Banks (64-MBIT)) on M4. M4 clock speed is 204MHz
Does any one have code to initialize this SDRAM on M4. Please share.

Thanks
Alastair
Labels (1)
0 Kudos
Reply
1 Reply

1,175 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Fri Jul 10 02:22:15 MST 2015
This is the memory type which is used on the LPC4350 Hitex board, so there is example code available, e.g. here:

http://www.lpcware.com/content/nxpfile/lpc4350apdlzip

Regards,
NXP Technical Support Team
0 Kudos
Reply