Need Help: Initalize IS42S16400J on LPC4357, M4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need Help: Initalize IS42S16400J on LPC4357, M4

1,228 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alastair on Tue Jun 23 02:17:24 MST 2015
Hi
I want to use SDRAM  IS42S16400J(1 Meg Bits x 16 Bits x 4 Banks (64-MBIT)) on M4. M4 clock speed is 204MHz
Does any one have code to initialize this SDRAM on M4. Please share.

Thanks
Alastair
标签 (1)
0 项奖励
回复
1 回复

1,181 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Fri Jul 10 02:22:15 MST 2015
This is the memory type which is used on the LPC4350 Hitex board, so there is example code available, e.g. here:

http://www.lpcware.com/content/nxpfile/lpc4350apdlzip

Regards,
NXP Technical Support Team
0 项奖励
回复