NXPUSBlib Example Virtual Serial

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXPUSBlib Example Virtual Serial

1,626件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nsacks on Mon Mar 25 09:10:42 MST 2013
Hello all,

For reference, I am working with LPC4330Xplorer board, trying to access the M4 core. I am also working in Linux.

I have been successful in downloading the Virtual Serial example project, however, when I go to test the echo functionality I am given the following script:

[  183.818893] usb 2-4: >config 1 interface 0 altsetting 0 endpoint 0x81 has an invalid bInterval 255, changing to 11

[  183.818906] usb 2-4: >config 1 interface 1 altsetting 0 bulk endpoint 0x3 has invalid maxpacket 16

[  183.818914] usb 2-4: >config 1 interface 1 altsetting 0 bulk endpoint 0x82 has invalid maxpacket 16

[  184.144427] usb 2-4: >New USB device found, idVendor=1fc9, idProduct=2047

[  184.144438] usb 2-4: >New USB device strings: Mfr=1, Product=2, SerialNumber=0

[  184.144445] usb 2-4: >Product: LPCUSBlib CDC Demo

[  184.144451] usb 2-4: >Manufacturer: NXP

[  184.157154] usb 2-4: >can't set config #1, error -32

mtp-probe: checking bus 2, device 2: "/sys/devices/pci0000:00/0000:00:13.2/usb2/2-4"

mtp-probe: bus: 2, device: 2 was not an MTP device

I was wondering if anyone new a solution to the problem, as I have exhausted all ideas. I have configured all linked projects correctly, but I think there might be a problem with the descriptor file, but I am not sure what to do with it.

Thanks!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,580件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nsacks on Tue Mar 26 21:17:28 MST 2013
I am using Ubuntu 12.10
0 件の賞賛
返信

1,580件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuong on Mon Mar 25 19:45:48 MST 2013
Hi,

Which Linux distri are you running? On our side, we have no problem running this example, from nxpUSBlib v0.98b, on Ubuntu 10.10 default USB driver.

With best regards,
0 件の賞賛
返信