NXP USB host lite for LPC17xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP USB host lite for LPC17xx

3,271 次查看
laurianus
Contributor I

Hi

Can you help me with a valid link for this (ChaN's FatFs implementation on NXP USB host lite for LPC17xx)? 

The old link does not work and I could not find it anywhere
http://www.siwawi.arubi.uni-kl.de/avr_projects/arm_projects/arm_memcards/index.html#chanfat_lpc_cm3


Thank you
Laurian

标签 (3)
标记 (3)
0 项奖励
回复
3 回复数

3,139 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I believe the link you provided is not belong to nxp. Was your mentioned demo code developed by nxp?

For NXP demo, we only has

AN10916: FAT library EFSL and FatFs port on NXP LPC1700:

http://www.nxp.com/documents/application_note/AN10916.zip

Have a nice day

Jun Zhang

0 项奖励
回复

3,140 次查看
laurianus
Contributor I

Thank you for your for My. I have that zip file but it is working only for SD Card and I need it to work on MSC USB Host... I saw in that deadlink was the code for this.

If some one can help me to do it I can pay for it.I need to able to read on lpc 1768 mcu small text files (less than 10K) from an USB drive (not sd card) with capacity larger than 8G (because i want to have usb C connector and because smaller usb drives are hard to find) so it needs to be Fat32. As I understand if fatfs it is implemented I can read files from an fat32 usb drive on lpc1768.

If some one can help me to do it I can pay for it.

Thank you 

0 项奖励
回复

3,140 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Laurian

I think the demo you are looking for is not nxp demo code. So I can't provide it to you.

Let's leave it here and see if anyone have it. 

Have a nice day

Jun Zhang

0 项奖励
回复