NXP Part numbering specifics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Part numbering specifics

ソリューションへジャンプ
17,194件の閲覧回数
mikesimmonds
Contributor III

When going to a supplier (Farnell UK) to price/order specific devices, I see that there are two

apparently identical entries with differing NXP part numbers.

In this case, LPC1313FBD48 and LPC1313FBD48,151.

They have the same specifications!

What is the meaning of the ",151" suffix?

Cheers, Mike.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
12,365件の閲覧回数
rolfmeeser
NXP Employee
NXP Employee

That's just the indication of packing method, like tray vs. reel. You can find a list of these codes here: http://www.nxp.com/documents/other/PackingLetterCodeusedinOrderablePartNumber.pdf

The three letter packing code is repeated in the last three digits of the twelve-digit "12NC" NXP ordering code. Parts with different packing options therefore have multiple ordering codes. For the LPC1313FBD48/01 there is apparently only one option: 9352 950 13151 indicates tray packing.

Be aware that besides the LPC1313/01 there is still the older LPC1313 for legacy projects!

Rolf

元の投稿で解決策を見る

1 返信
12,366件の閲覧回数
rolfmeeser
NXP Employee
NXP Employee

That's just the indication of packing method, like tray vs. reel. You can find a list of these codes here: http://www.nxp.com/documents/other/PackingLetterCodeusedinOrderablePartNumber.pdf

The three letter packing code is repeated in the last three digits of the twelve-digit "12NC" NXP ordering code. Parts with different packing options therefore have multiple ordering codes. For the LPC1313FBD48/01 there is apparently only one option: 9352 950 13151 indicates tray packing.

Be aware that besides the LPC1313/01 there is still the older LPC1313 for legacy projects!

Rolf