NXP Part numbering specifics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Part numbering specifics

Jump to solution
17,071 Views
mikesimmonds
Contributor III

When going to a supplier (Farnell UK) to price/order specific devices, I see that there are two

apparently identical entries with differing NXP part numbers.

In this case, LPC1313FBD48 and LPC1313FBD48,151.

They have the same specifications!

What is the meaning of the ",151" suffix?

Cheers, Mike.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
12,242 Views
rolfmeeser
NXP Employee
NXP Employee

That's just the indication of packing method, like tray vs. reel. You can find a list of these codes here: http://www.nxp.com/documents/other/PackingLetterCodeusedinOrderablePartNumber.pdf

The three letter packing code is repeated in the last three digits of the twelve-digit "12NC" NXP ordering code. Parts with different packing options therefore have multiple ordering codes. For the LPC1313FBD48/01 there is apparently only one option: 9352 950 13151 indicates tray packing.

Be aware that besides the LPC1313/01 there is still the older LPC1313 for legacy projects!

Rolf

View solution in original post

1 Reply
12,243 Views
rolfmeeser
NXP Employee
NXP Employee

That's just the indication of packing method, like tray vs. reel. You can find a list of these codes here: http://www.nxp.com/documents/other/PackingLetterCodeusedinOrderablePartNumber.pdf

The three letter packing code is repeated in the last three digits of the twelve-digit "12NC" NXP ordering code. Parts with different packing options therefore have multiple ordering codes. For the LPC1313FBD48/01 there is apparently only one option: 9352 950 13151 indicates tray packing.

Be aware that besides the LPC1313/01 there is still the older LPC1313 for legacy projects!

Rolf