NXP LPC Arm LCD compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP LPC Arm LCD compatibility

1,224 次查看
jonathansmith
Contributor III

I'm looking at starting some development using the LPC4357-K43WQA development board. It is for a project that needs an LCD screen. LPC ARM devices are what we have the most experience with here, so the development board that uses an LPC4357 and comes with an LCD screen looks like an obvious choice.

I see that it uses a K43WQA screen, but these aren't widely available and I would like to have a choice of screen sizes, and ones that are easier to source.

Is there an alternative screen that will work with the LPC4357? I can't work out what the interface is. If it's a standard interface then I guess I can have a choice of different screen sizes to work with?

Thanks in advance.

标签 (2)
0 项奖励
回复
0 回复数