NMI handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
8,812件の閲覧回数
andreiszeghy
Contributor I

Hello,

  I'm using an LPC1769 MCU and have pin P2[10] configured as an external interrupt.  I knew this pin was also the Non-Maskable Interrupt, but at the time I was sure that this pin would never be asserted during reset.  Well, of course, come to find out that on rare occasions this pin is triggered, and stays triggered,  when the MCU resets. So the code winds up locked in the NMI handler.

  I am not using the NIM otherwise and the handler currently looks like this:

void NMI_Handler(void)
{
    while(1) {}
}

  Is there anything I can do in the handler to manage the occasions when the MCU reset's with the NMI asserted?

Thanks, any info is greatly appreciated,

Andrei

0 件の賞賛
返信
1 解決策
8,475件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andrei Szeghy,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your description, it seems MCU won't boot up successfully on rare occasion because of P2[10] is 'triggered', is it right?
However, I don't agree with the reason you pointed out, I think the MCU enter into the ISP mode, to validate this assumption, please adding a pull-up resistor (10 KΩ) on the P2[10] pin to terminate this 'issue'。

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
8,475件の閲覧回数
andreiszeghy
Contributor I

Hi Jeremy,

   Thanks for the reply.  There already is a pull-up resistor in the circuit, the input being "triggered" is not a bug.  On occasion there is physically something in front of a sensor that I never anticipated being there. 

  My mistake, you are correct, I overlooked the ISP mode detail on that pin!  A lot of bad words are firing off in my head!  I don't think there is any way to get out of this scenario.  I'll have to make some non programmatic changes to work around this.

Thank you,

Andrei

0 件の賞賛
返信
8,476件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andrei Szeghy,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your description, it seems MCU won't boot up successfully on rare occasion because of P2[10] is 'triggered', is it right?
However, I don't agree with the reason you pointed out, I think the MCU enter into the ISP mode, to validate this assumption, please adding a pull-up resistor (10 KΩ) on the P2[10] pin to terminate this 'issue'。

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信