NHS3152: Program will only run while connected to LPC-link-2 & PC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS3152: Program will only run while connected to LPC-link-2 & PC

4,336 次查看
leo94
Contributor IV

Hello,

I am trying to use NHS3152 DEMO BOARD to read a resistance. 

The program works fine except an issue with the scale. 

I am now want to flash the program onto the NHS3152 DEMO board's chip, so that it can run without being connected to the PC and LPC-LINK2.

 

I am doing the following: 

1. Press flash icon and connect to emulator --> press OK

It opens Program Flash using LPC-LINK2 CMSIS-DAP V5.173

I chose: 
Options: 

  • Display progress log
  • Run flash command and copy to clipboard

Connect sctrip: ISPRestetConnect.scp

Flash driver: NSS_20k_8k_IAP.cfx

program flash memory

select file: ...\DAC_ADC_toghether.axf (see code at end of Quesiton) 

Erase Option: Mass erase

image.png

And pressed OK.

I get the following message out:  

 

 

 

Nc:verify offset 0x2400/0x45B0[0x400/0x400]
Ps: ( 57) at 00002400: 1024 bytes - 10240/17840
Nc:verify offset 0x2800/0x45B0[0x400/0x400]
Ps: ( 63) at 00002800: 1024 bytes - 11264/17840
Nc:verify offset 0x2C00/0x45B0[0x400/0x400]
Ps: ( 68) at 00002C00: 1024 bytes - 12288/17840
Nc:verify offset 0x3000/0x45B0[0x400/0x400]
Ps: ( 74) at 00003000: 1024 bytes - 13312/17840
Nc:verify offset 0x3400/0x45B0[0x400/0x400]
Ps: ( 80) at 00003400: 1024 bytes - 14336/17840
Nc:verify offset 0x3800/0x45B0[0x400/0x400]
Ps: ( 86) at 00003800: 1024 bytes - 15360/17840
Nc:verify offset 0x3C00/0x45B0[0x400/0x400]
Ps: ( 91) at 00003C00: 1024 bytes - 16384/17840
Nc:verify offset 0x4000/0x45B0[0x400/0x400]
Ps: ( 97) at 00004000: 1024 bytes - 17408/17840
Nc:verify offset 0x4400/0x45B0[0x1B0/0x400]
Ps: (100) at 00004400: 1024 bytes - 18432/17840
Nt: Erased/Wrote page  0-17 with 17840 bytes in 6667msec
Pb: (100) Finished writing Flash successfully.
Nt: Flash Write Done
Nt: Loaded 0x45B0 bytes in 7358ms (about 2kB/s)

 

 

 

 

At this point however if i bring the phone into the NFC range it reads: 
"Tag is empty or phone is not aligned" instead of the expected "res value is.. " 

The program works since if I run it via Debug session it runs. but even here if i disconnect the LPClink2 I get the same "tag is empty" message. 

 

Here is the code i am running: 

It essentially displays a message with the resistance when the field is present. 

 

 

 

/*
FROM https://community.nxp.com/t5/NFC/Measure-resistance-NHS3152/m-p/831045

1. Set the configuration of the analog pins to IOCON_FUNC_1
2. Connect the DAC to ANA1, set a continuous conversion of 1.25V.
3. Connect the I2D to ANA4, configure correctly and start a conversion. Only when a conversion is started, current will start flowing over your resistor. The current will continue to flow when the conversion ends. -> a
4. Connect the ADC to ANA4, and measure the voltage. -> v4
5. Connect the ADC to ANA1, and measure the voltage. -> v1

*/




/* ------------------------------------------------------------------------- */

#include <string.h>
#include <stdlib.h>
#include <stdio.h> // contains sprintf function (needs to be included to avoid : https://stackoverflow.com/questions/8440816/warning-implicit-declaration-of-function
#include "board.h"
#include "ndeft2t/ndeft2t.h"

/* ------------------------------------------------------------------------- */

#define LOCALE "en" /**< Language used when creating TEXT records. */
#define MIME "nhs31xx/example.ndef" /**< Mime type used when creating MIME records. */

/** The URL will be used in a single-record NDEF message. */
#define MAX_URI_PAYLOAD (254 - NDEFT2T_MSG_OVERHEAD(true, NDEFT2T_URI_RECORD_OVERHEAD(true)))
static const uint8_t sUrl[MAX_URI_PAYLOAD + 1 /* NUL */] = "nxp.com/NTAGSMARTSENSOR";

/**
* The text and the MIME data are always presented together, in a dual-record NDEF message.
* Payload length is split evenly between TEXT and MIME.
*/
#define MAX_TEXT_PAYLOAD (254 - (NDEFT2T_MSG_OVERHEAD(true, \
NDEFT2T_TEXT_RECORD_OVERHEAD(true, sizeof(LOCALE) - 1) + \
NDEFT2T_MIME_RECORD_OVERHEAD(true, sizeof(MIME) - 1)) / 2))
static uint8_t sText[MAX_TEXT_PAYLOAD] = "10 V1-V4";

/** @copydoc MAX_TEXT_PAYLOAD */
#define MAX_MIME_PAYLOAD MAX_TEXT_PAYLOAD
static uint8_t sBytes[MAX_MIME_PAYLOAD] = {0, 0xAA, 0xBB, 0xCC, 0xDD, 0xEE};

/* ------------------------------------------------------------------------- */

/**
* Used to determine which NDEF message must be generated.
* - @c true: generate a single-record NDEF message containing a URL.
* - @c false: generate a dual-record NDEF message containing a TEXT and a MIME record.
*/
static bool sState;

static volatile bool sButtonPressed = false; /** @c true when the WAKEUP button is pressed on the Demo PCB */
static volatile bool sMsgAvailable = false; /** @c true when a new NDEF message has been written by the tag reader. */
static volatile bool sFieldPresent = false; /** @c true when an NFC field is detected and the tag is selected. */

static void GenerateNdef_Url(void);
static void GenerateNdef_TextMime(void);
static void ParseNdef(void);

/* ------------------------------------------------------------------------- */

//Store adc_1, adc_4, current and resistance value
static volatile float adcInput_4 = 5.0; // 4. store V input 4
static volatile float adcInput_1 = 5.0; // 5. store V input 1
static volatile int current_native; // 3. store I2D ana 4
static volatile int current_picoampere; // 3. store I2D ana4
static volatile double resval = -1; // store resistance calculated: (dcInput_1-adcInput_4)/Current_picoampere*10e-6

static void adcdac_nss_example_1(void); //continuous DAC ana1
static void i2d_nss_example_1(void); //I2D ana4
static void adcdac_nss_example_3(void); //NEW single shot get ADC value ana4
static void adcdac_nss_example_3_2(void); //NEW single shot get ADC value ana1


/**
* Handler for PIO0_0 / WAKEUP pin.
* Overrides the WEAK function in the startup module.
*/
void PIO0_IRQHandler(void)
{
Chip_GPIO_ClearInts(NSS_GPIO, 0, 1);
sButtonPressed = true; /* Handled in main loop */
}

/**
* Called under interrupt.
* @see NDEFT2T_FIELD_STATUS_CB
* @see pNdeft2t_FieldStatus_Cb_t
*/
void App_FieldStatusCb(bool status)
{
if (status) {
LED_On(LED_RED);
}
else {
LED_Off(LED_RED);
}
sFieldPresent = status; /* Handled in main loop */
}

/**
* Called under interrupt.
* @see NDEFT2T_MSG_AVAILABLE_CB
* @see pNdeft2t_MsgAvailable_Cb_t
*/
void App_MsgAvailableCb(void)
{
sMsgAvailable = true; /* Handled in main loop */
}

/* ------------------------------------------------------------------------- */

/** Generates a single-record NDEF message containing a URL, and copies it to the NFC shared memory. */
static void GenerateNdef_Url(void)
{
uint8_t instance[NDEFT2T_INSTANCE_SIZE];
uint8_t buffer[NFC_SHARED_MEM_BYTE_SIZE];
NDEFT2T_CREATE_RECORD_INFO_T recordInfo = {.pString = NULL /* don't care */,
.shortRecord = true,
.uriCode = 0x01 /* "http://www." */};
NDEFT2T_CreateMessage(instance, buffer, NFC_SHARED_MEM_BYTE_SIZE, true);
if (NDEFT2T_CreateUriRecord(instance, &recordInfo)) {
if (NDEFT2T_WriteRecordPayload(instance, sUrl, (int)strlen((char *)sUrl))) {
NDEFT2T_CommitRecord(instance);
}
}
NDEFT2T_CommitMessage(instance); /* Copies the generated message to NFC shared memory. */
}

/** Generates a dual-record NDEF message containing a TEXT and a MIME record, and copies it to the NFC shared memory. */
static void GenerateNdef_TextMime(void)
{
uint8_t instance[NDEFT2T_INSTANCE_SIZE];
uint8_t buffer[NFC_SHARED_MEM_BYTE_SIZE];
NDEFT2T_CREATE_RECORD_INFO_T textRecordInfo = {.pString = (uint8_t *)"en" /* language code */,
.shortRecord = true,
.uriCode = 0 /* don't care */};
NDEFT2T_CREATE_RECORD_INFO_T mimeRecordInfo = {.pString = (uint8_t *)MIME /* mime type */,
.shortRecord = true,
.uriCode = 0 /* don't care */};
NDEFT2T_CreateMessage(instance, buffer, NFC_SHARED_MEM_BYTE_SIZE, true);
if (NDEFT2T_CreateTextRecord(instance, &textRecordInfo)) {
if (NDEFT2T_WriteRecordPayload(instance, sText, sizeof(sText) - 1 /* exclude NUL char */)) {
NDEFT2T_CommitRecord(instance);
}
}
if (NDEFT2T_CreateMimeRecord(instance, &mimeRecordInfo)) {
if (NDEFT2T_WriteRecordPayload(instance, sBytes, sizeof(sBytes))) {
NDEFT2T_CommitRecord(instance);
}
}
NDEFT2T_CommitMessage(instance); /* Copies the generated message to NFC shared memory. */
}

/** Parses the NDEF message in the NFC shared memory, and copies the TEXT and MIME payloads. */
static void ParseNdef(void)
{
uint8_t instance[NDEFT2T_INSTANCE_SIZE];
uint8_t buffer[NFC_SHARED_MEM_BYTE_SIZE];
NDEFT2T_PARSE_RECORD_INFO_T recordInfo;
int len = 0;
uint8_t *pData = NULL;

if (NDEFT2T_GetMessage(instance, buffer, NFC_SHARED_MEM_BYTE_SIZE)) {
while (NDEFT2T_GetNextRecord(instance, &recordInfo) != false) {
pData = (uint8_t *)NDEFT2T_GetRecordPayload(instance, &len);
switch (recordInfo.type) {
case NDEFT2T_RECORD_TYPE_TEXT:
if ((size_t)len <= MAX_TEXT_PAYLOAD) {
memcpy(sText, pData, (size_t)len);
memset(sText + len, 0, MAX_TEXT_PAYLOAD - (size_t)len);
}
break;
case NDEFT2T_RECORD_TYPE_MIME:
if ((size_t)len <= MAX_MIME_PAYLOAD) {
memcpy(sBytes, pData, (size_t)len);
memset(sBytes + len, 0, MAX_MIME_PAYLOAD - (size_t)len);
}
break;
default:
/* ignore */
break;
}
}
}
}


// 1. Set the configuration of the analog pins to IOCON_FUNC_1
// 2. Connect the DAC to ANA1, set a continuous conversion of 1.25V.

void adcdac_nss_example_1(void) // Modified IOCON_ANA0_0 --> IOCON_ANA0_1 & ADCDAC_IO_ANA0_0 --> ADCDAC_IO_ANA0_1
{
//! [adcdac_nss_example_1]
Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_1, IOCON_FUNC_1); // IOCON_FUN_1
Chip_ADCDAC_Init(NSS_ADCDAC0);
Chip_ADCDAC_SetMuxDAC(NSS_ADCDAC0, ADCDAC_IO_ANA0_1);
Chip_ADCDAC_SetModeDAC(NSS_ADCDAC0, ADCDAC_CONTINUOUS);
Chip_ADCDAC_WriteOutputDAC(NSS_ADCDAC0, 3000);
//! [adcdac_nss_example_1]
}


/* ------------------------------------------------------------------------- */
// 3. Connect the I2D to ANA4, configure correctly and start a conversion. Only when a conversion is started, current will start flowing over your resistor. The current will continue to flow when the conversion ends. -> a

// FROM i2d_nss_example_1


void i2d_nss_example_1(void)
{
//! [i2d_nss_example_1]
int i2dValue;
int i2dNativeValue;
Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_4, IOCON_FUNC_1); // IOCON_FUN_1
Chip_I2D_Init(NSS_I2D);
Chip_I2D_Setup(NSS_I2D, I2D_SINGLE_SHOT, I2D_SCALER_GAIN_10_1, I2D_CONVERTER_GAIN_LOW, 100);
Chip_I2D_SetMuxInput(NSS_I2D, I2D_INPUT_ANA0_4);
Chip_I2D_Start(NSS_I2D);
while (!(Chip_I2D_ReadStatus(NSS_I2D) & I2D_STATUS_CONVERSION_DONE)) {
; /* wait */
}
i2dNativeValue = Chip_I2D_GetValue(NSS_I2D);
i2dValue = Chip_I2D_NativeToPicoAmpere(i2dNativeValue, I2D_SCALER_GAIN_10_1, I2D_CONVERTER_GAIN_HIGH, 100);
Chip_I2D_DeInit(NSS_I2D);
//! [i2d_nss_example_1]

current_native = i2dNativeValue;
current_picoampere = i2dValue;
}

// 4. Connect the ADC to ANA4, and measure the voltage. -> v4

//FROM Example 3 - Single-shot Analog-to-Digital Conversion without IRQ

// The conversion: adc_input_voltage = (native_value * 1.2V) / 2825 + 0.09V
void adcdac_nss_example_3(void) // Modifications: IOCON_ANA0_5--> IOCON_ANA0_4 & converted adcinput_4= (adcInput_4 * 1.2) / 2825 + 0.09
{
//! [adcdac_nss_example_3]
Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_4, IOCON_FUNC_1);
//Chip_ADCDAC_Init(NSS_ADCDAC0);
Chip_ADCDAC_SetMuxADC(NSS_ADCDAC0, ADCDAC_IO_ANA0_4);
Chip_ADCDAC_SetInputRangeADC(NSS_ADCDAC0, ADCDAC_INPUTRANGE_WIDE);
Chip_ADCDAC_SetModeADC(NSS_ADCDAC0, ADCDAC_SINGLE_SHOT);
Chip_ADCDAC_StartADC(NSS_ADCDAC0);

while (!(Chip_ADCDAC_ReadStatus(NSS_ADCDAC0) & ADCDAC_STATUS_ADC_DONE)) {
; /* Wait until measurement completes. For single-shot mode only! */
}

adcInput_4 = Chip_ADCDAC_GetValueADC(NSS_ADCDAC0);
adcInput_4= (adcInput_4 * 1.2) / 2825 + 0.09; // CONVERSION added line

//! [adcdac_nss_example_3]
}


void adcdac_nss_example_3_2(void) // Modifications: IOCON_ANA0_5--> IOCON_ANA0_1 & converted adcinput_1= (adcInput_1 * 1.2) / 2825 + 0.09
{
//! [adcdac_nss_example_3]
Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_1, IOCON_FUNC_1);
//Chip_ADCDAC_Init(NSS_ADCDAC0);
Chip_ADCDAC_SetMuxADC(NSS_ADCDAC0, ADCDAC_IO_ANA0_1);
Chip_ADCDAC_SetInputRangeADC(NSS_ADCDAC0, ADCDAC_INPUTRANGE_WIDE);
Chip_ADCDAC_SetModeADC(NSS_ADCDAC0, ADCDAC_SINGLE_SHOT);
Chip_ADCDAC_StartADC(NSS_ADCDAC0);

while (!(Chip_ADCDAC_ReadStatus(NSS_ADCDAC0) & ADCDAC_STATUS_ADC_DONE)) {
; /* Wait until measurement completes. For single-shot mode only! */
}

adcInput_1 = Chip_ADCDAC_GetValueADC(NSS_ADCDAC0);
adcInput_1= (adcInput_1 * 1.2) / 2825 + 0.09; // CONVERSION added line

//! [adcdac_nss_example_3]
}





// MAIN
int main(void)
{
Board_Init();
NDEFT2T_Init();
NVIC_EnableIRQ(PIO0_IRQn); /* PIO0_IRQHandler is called when this interrupt fires. */
Chip_GPIO_EnableInt(NSS_GPIO, 0, 1);


// for ever, WHILE field is detected: 2. Connect the DAC to ANA1, set a continuous conversion of 1.25V.
for (;;) {
while (sFieldPresent) {

// 2. Connect the DAC to ANA1 -output Voltage
adcdac_nss_example_1();
// 3. Connect the I2D to ANA4, - read current ana4 through resistor
i2d_nss_example_1();
// 4. Connect the ADC to ANA4, and measure the voltage. ->v4
adcdac_nss_example_3();
// 5. Connect the ADC to ANA1, and measure the voltage. -> v1
adcdac_nss_example_3_2();
// generate the message only once per field???
GenerateNdef_TextMime();
resval = (adcInput_1-adcInput_4)/(current_picoampere * 1e-12); // (v1-v4)/(I4pico * 1e-12) V/I=R [V/A =ohm]
sprintf((char *)sText, "adc_1: %6.2f adc_4: %6.2f current_picoampere: %8.d resistance: %e current_native: %6.d", adcInput_1, adcInput_4,current_picoampere, resval,current_native );//commented in from Thesis, changes payloadText to sText

}
//Chip_PMU_PowerMode_EnterDeepSleep();
}
return 0;
}

 

 

 

  

0 项奖励
回复
6 回复数

4,299 次查看
driesmoors
NXP Employee
NXP Employee

You can instrument your code, to toggle a pin (or led) demonstrating your code is running.

The NHS3152 IC has a type 2 interface NFC controller built-in: this means that the NDEF message must have been copied to the NFC memory in time. There is no way to delay reading by the phone. It may be that your NDEF message is made available too late.

With your program battery powered, do you see the old message when you tap a second time? Which phone do you use? Different Android phones have vastly different timings when it comes to enabling the field and starting to read the NFC memory.

 

0 项奖励
回复

4,331 次查看
converse
Senior Contributor V

Suggest you read this FAQ

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-is-Semihosting/m-p/475390

 

especiially the Important notes on Semihosting section

4,328 次查看
leo94
Contributor IV

Thanks! 

So since i have ran it as a debug, it will no loger work standalone. 
So my next question is:
What steps do i need to take to get i to work standalone?

0 项奖励
回复

4,324 次查看
converse
Senior Contributor V

remove semihosting...

Note that it is not that you have built it for debug that it is not running, it is the semihosting (which requires a debugger attached) that is stopping it.

0 项奖励
回复

4,309 次查看
leo94
Contributor IV

Ok, how do i remove semihosting ? 

Is it a specific command? or do i just attach the NHS3152 to the PC via some type of cable? 

 

0 项奖励
回复

4,302 次查看
driesmoors
NXP Employee
NXP Employee

Adding/removing semihosting is done via the project settings, and removing any printf calls you have in your code. 

0 项奖励
回复