NGX LPC1857 Header Board. Can't Flash or JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NGX LPC1857 Header Board. Can't Flash or JTAG

1,344件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Sat Jan 25 16:44:26 MST 2014
I have a new out of the box NGX LPC1857 board. I am using it with LPCXpresso and LPC-Link JTAG board.

I have built the NGX supplied projects, but when I go to flash them I get and error

Failed on connect: Ep(01). Target marked as not debuggable.
Connected. Was: None. DpID:     EDB6. Info: HID64HS12[/color]

The detailed error message is:

crt_emu_lpc18_43_nxp -flash-load-exec "C:\Temp\workspace18\periph_atimer\Debug\periph_atimer.axf" -g -2 -vendor=NXP -
pLPC1830 -wire=hid -s250 -flash-driver=LPC18_43_SPIFI_4MB_64KB.cfx -x C:/Temp/workspace18/periph_atimer/Debug

Ni: LPCXpresso Debug Driver v6.0 (Dec 30 2013 11:03:08 - crt_emu_lpc18_43_nxp.exe build 1222)
Pc: (  0) Reading remote configuration
Nc: Found chip XML file in C:/Temp/workspace18/periph_atimer/Debug/LPC1830.xml
Pc: (  5) Remote configuration complete
Pc: ( 15) nSRST assert (if available)
Ed:02: Failed on connect: Ep(01). Target marked as not debuggable.
Et: Emu(0): Connected. Was: None. DpID:     EDB6. Info: HID64HS12
Error 0: (null)
Last sticky: 0. AIndex: 0
No MemAp selected

I have no problem in using the LPC-Link on a LPC1769.
No Speed test
SWD Frequency: 50 KHz. RTCK: False. Vector catch: False.
Packet delay: 0  Poll delay: 0.
Pc: (100) Target Connection Failed

The NGX projects for the 1857 come with the MCU set for 18230. I have tried changing the MCU settings to 1857 but get the same result.

I would appreciate any suggestions or help.

Thanks.

Dave Sidlauskas
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Sun Jan 26 16:41:54 MST 2014
Thanks for the FAQS.

It turns out it was a hardware problem. The 10 pin JTAG provided by UcPros had the red stripe on pin 16 instead of pin 1.

Also, this board comes with a built-in self-test program. One of the tests is an Ethernet test. I spent a lot of time trying to get this to work before learning from NGX that the test firmware is defective. A note in the box would have been nice.
0 件の賞賛
返信

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Jan 26 03:22:55 MST 2014
http://www.lpcware.com/content/faq/lpcxpresso/target-marked-not-debuggable
0 件の賞賛
返信