Is there any development boards with LPC1857 which will support IAR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any development boards with LPC1857 which will support IAR?

2,698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by microeval on Sun Sep 29 23:26:59 MST 2013
Hi All,

I am new to the NXP-LPC platform.
Is there any development board which will support SPI and USART connectivity with IAR workbench?.
I want to use SPI connectivity from the board to my external SPI slave device.

Any release note related to LPC1857 board for SPI.

Thanks,
Ram.
Labels (1)
0 Kudos
Reply
6 Replies

2,673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Oct 03 11:37:20 MST 2013
The ULink-ME debugger is not compatible with IAR tools.  You have a few choices:
1. Purchase a J-Link debugger (http://www.segger.com/j-link-oem-versions.html)
2. Purchase an LPC-Link2 (http://www.nxp.com/demoboard/OM13054.html)
0 Kudos
Reply

2,673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by microeval on Thu Oct 03 07:29:57 MST 2013
Hi bavarian & MC,

I selected the NGX Development board: followed this link

http://ngxtech.com/knowledgebase/index.php?title=LPC1830-Xplorer_Quick_Start_Guide

But this link gives the idea with the keil-MDK(Debugger they are used is ULINK-ME, but this debugger is not present in IAR project->options->Debugger->Driver) support.
Can't we use the j-Link as the debugger in IAR for this board? Is there any other Debugger we can use for this board.?

Thanks,
Ram.


0 Kudos
Reply

2,673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by microeval on Thu Oct 03 05:03:33 MST 2013
Thank you very much bavarian,

I downloaded the LPC18xx part number code and customizing for my application.

Thanks,
Ram. 

0 Kudos
Reply

2,673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Oct 01 05:32:37 MST 2013
Please use this link:

http://lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers

Only the dot at the end of the link was wrong.

0 Kudos
Reply

2,674 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by microeval on Mon Sep 30 21:54:53 MST 2013
Hi MC,

Thanks for your reply,

I tryed this link:
http://lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers.

Am getting : Error - missing page or bad link.

Can please give me correct link and suggestions.

Thanks,
Ram.
0 Kudos
Reply

2,673 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Sep 30 07:32:10 MST 2013
Hi Ram,
You can use MCB1857 see here
http://www.keil.com/mcb1800/MCB1800v1-3-schematics.pdf

For software examples, please go through LPCopen platform.
http://lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers.
After downloading LPCOpen extract and find the IAR Embedded Workbench examples in the folder
..\lpcopen\applications\lpc18xx_43xx\iar_ewarm_projects

Hope it helps
MC
0 Kudos
Reply