NAND-flash and LPC1857

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND-flash and LPC1857

1,130件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by WOVAN on Fri Jul 11 05:05:35 MST 2014
Hi,

i'm designing a datalogger with the LPC1857. I need 1Gbyte of logmemory. i see the lpc 1857 can't address this amount so i'm looking into a  NAND flash. But it is unclear to me if the EMC of the LPC1857 can work with a NAND-flash. and if so, are there any design examples available?

kind regards,

Wouter
ラベル(1)
0 件の賞賛
返信
1 返信

1,106件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Fri Jul 11 06:52:18 MST 2014
You should be able to add NAND flash to the EMC.
But: you need a complex piece of software to access the NAND flash!
My advice: don't do that!

Instead: use a microSD card. No pain, you can adjust the storage size by requirement, you can change the card and put it into your PC.

If you want a non-replaceable solution, try a emmc.

regards
Wolfgang

0 件の賞賛
返信