NAND Flash interface support in LPC4367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NAND Flash interface support in LPC4367

4,642 次查看
akhilesh_sreedh
Contributor III

Hello,

The External memory controller section in LPC4367's datasheet specifies only SRAM, ROM, NOR flash and SDRAM devices to be connected to the EMC. 

However, is there any way to interface a NAND Flash to LPC4367 having the following interface?

pastedImage_1.png

Thanks and Regards,

Akhilesh Sreedharan

标记 (3)
0 项奖励
回复
6 回复数

4,240 次查看
leecoakley
Contributor III

Waveshare make a 4357-based board with a NAND chip on it and they provide an example driver in their demo package.  Could be a useful example to look at.

0 项奖励
回复

4,240 次查看
akhilesh_sreedh
Contributor III

The link doesn't seem to be working, please share the files. 

0 项奖励
回复

4,239 次查看
leecoakley
Contributor III

I will share it, but you can just google "Waveshare Open4357-C" for the site.

See attached zip. The NAND code is under /examples waveshare/EMC/EMC_NANDFLASH/

0 项奖励
回复

4,239 次查看
akhilesh_sreedh
Contributor III

Hello Bernhard Fink,

Thanks a lot for the reply. 

The OP of the link which you have suggested asks if an SDRAM and NAND both can be interfaced simultaneously to the EMC. We have a similar system which will have a SDRAM and NAND.

Can you please let us know if there will be a need to re-initialize the EMC register when there is a switch between SDRAM and NAND as NAND read/write is a software controlled process and SDRAM read/write will be managed by the External memory controller. 

Thanks,

Akhilesh Sreedharan

0 项奖励
回复

4,239 次查看
bernhardfink
NXP Employee
NXP Employee

On the LPC4300 SDRAM and SRAM interface are two different instances with own register settings. No problem to connect a memory device to both, no dynamic changes are required at runtime.

Regards,

Bernhard.

4,239 次查看
bernhardfink
NXP Employee
NXP Employee

It should be possible to interface a NAND flash, as long as you find a driver for it.

But it's a sw managed read/write process, you will not be able to boot or execute from it.

There is a NAND driver for the LPC1788, which could most likel y be adapted to the LPC4300 platform:

https://community.nxp.com/thread/418534 

Regards,

Bernhard.

0 项奖励
回复