Multi layer support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi layer support

1,405件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Flo on Tue Jan 07 03:33:02 MST 2014
Hi there,

I was just wondering if the lpc4357 lcd controller supports multi layer features.
Until now I've been working with a single layer using the emwin gui. Now I wanted to use two layers,
but I'm getting trouble. I've taken a look into the datasheets and google, but found no hint about this.

Regards,
Florian
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,394件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Flo on Tue Jan 07 05:16:42 MST 2014
Ah ok,
thank you for this information.

Regards,
Florian

0 件の賞賛
返信

1,394件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Jan 07 04:29:54 MST 2014
Hello Florian,

the LCD controller inside our MCUs does not support multiple layers or displays.
We can only generate one sort of timing, but even if you would two identical displays (or use one with two layers) the DMA cannot be controlled in such a way that each display gets its own data.
So even with a little bit help from software and maybe some external hardware you will not be able to put something reasonable together.

Regards,
NXP Support Team
0 件の賞賛
返信