Multi layer support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi layer support

1,407 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Flo on Tue Jan 07 03:33:02 MST 2014
Hi there,

I was just wondering if the lpc4357 lcd controller supports multi layer features.
Until now I've been working with a single layer using the emwin gui. Now I wanted to use two layers,
but I'm getting trouble. I've taken a look into the datasheets and google, but found no hint about this.

Regards,
Florian
标签 (1)
0 项奖励
回复
2 回复数

1,396 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Flo on Tue Jan 07 05:16:42 MST 2014
Ah ok,
thank you for this information.

Regards,
Florian

0 项奖励
回复

1,396 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Jan 07 04:29:54 MST 2014
Hello Florian,

the LCD controller inside our MCUs does not support multiple layers or displays.
We can only generate one sort of timing, but even if you would two identical displays (or use one with two layers) the DMA cannot be controlled in such a way that each display gets its own data.
So even with a little bit help from software and maybe some external hardware you will not be able to put something reasonable together.

Regards,
NXP Support Team
0 项奖励
回复