Missing files when Using IR Sample code on LPC812MAX through Keil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing files when Using IR Sample code on LPC812MAX through Keil

1,406件の閲覧回数
chenyirock
Contributor I

Hi I download the IR remote controller/ receiver example form the following website.

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-corte...

I downloaded Keil version 5 to run the project which is version 4 project. Hence I downloaded the legacy support in order to open version 4 project in Keil as shown in the attached picture. 

I think there should be more c and h files instead of just files related to GPIO. Like lpc8xx_mrt.c, lpc8xx_uart.c, lpc8xx_sct.c etc. 

pastedImage_4.jpg

Could you help me on this? Thank you very much!

ラベル(1)
0 件の賞賛
返信
1 返信

1,315件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Chen yi,

   No, the project is correct, no files is missing.

  If you check the AN11511_1.pdf, you will also find it is correct, please check this block diagram:

pastedImage_1.png

It use the SCT, gpio to realized it.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信