Microcontroller programming using LPC-link2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microcontroller programming using LPC-link2

2,241件の閲覧回数
vojtechbures
Contributor I

Hello,

I have LPC1768FBD100 mounted on PCB. I connect to this PCB using LPC-Link 2. When I run the CrossWorks program, I can communicate with this microcontroller (LPC1768FBD100) on the PCB and I can upload my program to it. But when I run the LPCScrypt program and try to write the program to my LPC1768FBD100 microcontroller with it, the program does not find it. It finds a single LPC4370 microcontroller, which is part of the LPC-Link 2 kit. I can easily write and read on the LPC4370. But I need to write to LPC1768FBD100 using the LPCScrypt program, which will not find my program with any combination of jumpers J1 and J2. Is it possible to write to the LPC1768FBD100 microcontroller using the LPCScrypt using the LPC-Link 2 kit? If so, what am I doing wrong, does anyone have an idea?
Is there a free program for commercial use that can do this?

Thank you very much.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,189件の閲覧回数
Ray_V
Contributor V

You can use the LPC-Link2 board to program the LPC1700 series using MCUXpresso IDE

0 件の賞賛
返信

2,223件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

LPCScrypt is a command-line based, fast flash, EEPROM, OTP and security programming tool for LPC1800 and LPC4300 series microcontrollers.

It is not for LPC1700.
See:
https://www.nxp.com/design/microcontrollers-developer-resources/lpcscrypt-v2-1-2:LPCSCRYPT

If we want to program LPC1700, Please use FlashMagic
https://www.flashmagictool.com/

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信