Memory space problem LPC1114/333

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory space problem LPC1114/333

1,905件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ALERICO90 on Fri Jul 10 06:24:52 MST 2015
Hello I hace a problem with my LPC1114/333, this LPC has 56K flash memory but I only can flash near 32K of the memory not even close to 56K.. what can I do?, I put the correct devive on keil uvision and still I can't flas more than 32K. Here is a screen capture of my target options
ラベル(1)
0 件の賞賛
返信
1 返信

1,887件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jul 10 14:49:46 MST 2015
Hi,

Please check the flash drivers used in Utilites->Settings. The Flash driver should be 56 Kb  i.e. LPC1xxx_56.FLM.

Thanks
NXP Technical Support
0 件の賞賛
返信