Meaning of the model name of the microcomputer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Meaning of the model name of the microcomputer

2,436 Views
atsuyosano
Contributor I

I am considering replacing the LPC microcomputer
What is the difference, such as ‘FBD’ and ‘JBD’ in the model name of the microcomputer?

I want to know the meaning of the alphabet used in the model name
If there is any material somewhere, please let me know.
Thank you.

 

LPCマイコンの置き換えを検討しています
マイコンの型名にある ’FBD’ ’JBD’ など 何が違うのでしょう。

型名に使用されている アルファベットの意味が知りたいです
どこかに資料があるのなら それも 教えていただきたいです
よろしくお願いいたします。

0 Kudos
Reply
7 Replies

2,414 Views
atsuyosano
Contributor I

thank you for your reply.
But not whether it can be physically replaced
I would like to know if it can be replaced in terms of performance.
for example
’Temperature range 40 ° C to 105 ° C’
’Temperature range 40 ° C to +85 ° C’

Please let me know if there is any material that describes the meaning of the alphabet of the model name.

 

返信ありがとうございます。
しかし、物理的に交換ができるかどうかでなく
性能的に交換ができるかを知りたいのです。
例えば
’Temperature range 40 °C to 105 °C’
’Temperature range 40 °C to +85 °C’

型名のアルファベットの意味を記している資料があれば 教えてください

0 Kudos
Reply

2,393 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello, 

 

I confirmed with out internal team, yes, 

 the different is FBD for -40 C to +85 C, JBD for  for -40 C to +105 C. 

 

Hope it helps.

 

Regards,

Alice

0 Kudos
Reply

2,403 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Which chip do you want to replace?

0 Kudos
Reply

2,382 Views
atsuyosano
Contributor I

hello.
Where can I find materials that explain the meaning of the model name alphabet?

こんにちは。
モデル名のアルファベットの意味を説明する資料は どこにありますか?

0 Kudos
Reply

2,361 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello atsuyosano,

There isn't, I got this information just from our internal SE team.

 

BR

Alice

0 Kudos
Reply

2,336 Views
atsuyosano
Contributor I

thank you very much

0 Kudos
Reply

2,420 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello, 

 

They are all "plastic low profile quad flat package", you can replace.

 

BR

Alice

0 Kudos
Reply