Mask vs disable interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mask vs disable interrupts

3,413件の閲覧回数
zorandjokic
Contributor II

I am working with LPC2378. I would like to mask (not disable) timer interrupt (10ms) during few instructions and than to unmusk it, so if timer interrupt happens during execution of those instructions, CPU would enter timer int. routine, after being unmasked.

Could it be done with this ARM device ? The same question regarding UARTs.

Thanks

タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,036件の閲覧回数
zorandjokic
Contributor II

A little test that I've made can be described with next pseudocode lines:

--- Init UART0 and define int. routine ---
VICSWPrioMask &= ~(1<< VICVectPriority6); //mask
--- wait for (devel. board) key press ---
VICSWPrioMask |= (1<< VICVectPriority6); //unmask
while(1){}

After CPU RESET, processor is waiting for key to be pressed. Using terminal
program, I've sent single character from PC, after which I pressed the key.
When processor passes "unmask" part of code it branches to interrupt routine.


Regards

0 件の賞賛
返信

3,036件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Zoran Djokic,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1) Could it be done with this ARM device ?
ARM7 architecture doesn't seem to support to suspend the masked interrupt, then execute it after be unmasked.
Hope this is clear.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信