Mac OS X (M1 Chip) MCUXPresso LinkServer not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mac OS X (M1 Chip) MCUXPresso LinkServer not working.

3,677 Views
dhjeong
Contributor II
hello. I am using MCUXpresso tool on M1 Mac OS.

But when I start debugging the project I get an error because LinkServer cannot be started.

Attach a screenshot. Is there any workaround for this?

MCUXpresso uses version 11.5.1.
0 Kudos
Reply
1 Reply

3,656 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @dhjeong it looks a problem with a permission in linux, when you connect your board, what you have log?(dmesg using the terminal) I mean, if you connect the board, did you have all the information about the board that you connect? If not, in linux, you need to check the rules (/etc/dev/rules/) i think, is equal in mac.

But if you have all information, maybe is about permission, open the rules and change the permissions or open the MCUXpresso as a superuser

0 Kudos
Reply