MRT has only 24 bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MRT has only 24 bit

1,300件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ER-Berlin on Thu Feb 27 05:44:20 MST 2014
I love the simple to use MRT-Timer on the LPC8xx controller. I was happy to read that this timers are also implemented in the new LPC15xx controllers. But WHY are the timer registers only 24 bit wide? With a 72 MHz system clock the longest timeout possible is only 233 ms. This is too short for most applications, e.g. serial receive timeout. Now i have to learn the use of SCT for longer timeouts.

Greetings from germany, Erwin
ラベル(1)
0 件の賞賛
返信
1 返信

1,282件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Feb 27 06:53:35 MST 2014

Quote: ER-Berlin
...longer timeouts.



And the winner is...................RIT  :O


Quote:
Chapter 20: LPC15xx Repetitive Interrupt Timer (RIT)

20.2 Features
• [color=#f00]48-bit[/color] counter



Perhaps your lost bits are there?
0 件の賞賛
返信