MFRC522

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFRC522

3,945 次查看
NFortunati
Contributor I

Hello, I am communicating because I have a problem using the MFRC522 with the LCP845-BRK.

I'm trying to do the AUTOTEST as the datasheet explains, and I can't get it to work. I am sending you the code so you can see if anyone realizes that I am doing wrong. 

I am using MCUXpresso as IDE.

Thank you very much, I am waiting

0 项奖励
回复
1 回复

3,931 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @NFortunati ,

 

Have you check the FIFOLEVELREG after perform 25 bytes writing? Have you check this register after starting the self test? BTW, how did you perform the softreset on RC522? by the command or by the reset pin? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复