MCUxpresso IDE CDT error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUxpresso IDE CDT error

2,111 Views
soleman
Contributor I

Hi,

   i am using MCUxpresso IDE for the board LPC55S36. I was creating new folder and files for my project development, when i tried to add folder path in project properties suddenly got a issue as "The Project is not a CDT project". previously i did file adding and path adding it was working fine.

now if i try to open other example project then also the same error showing.

How can i solve the issue can anyone help?

Thank you.

0 Kudos
Reply
3 Replies

2,073 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel and I will be supporting your case, maybe this post could help you.

Custom C/C++ Headers with Eclipse | MCU on Eclipse

Best regards,
Pavel

0 Kudos
Reply

1,985 Views
soleman
Contributor I

Hi Pavel, 

              Thank you so much for the reply. I followed that same process to create new file and folder. I want to know how to recover the project from CDT error. Because after implementing a large part of my application if i get the CDT error it will be difficult to rewrite the application from starting. Please help.

 

Best Regards 

Soleman

 

0 Kudos
Reply

1,953 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you add an image of the error pop-up, and the message shows it on the console IDE?

What is the version of SDK and the IDE?

Best regards,
Pavel

0 Kudos
Reply