MCUXpresso Sugger image Linit 512k

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Sugger image Linit 512k

1,403件の閲覧回数
jongsubkim
Contributor II

My Device Config( MCUXpresso 11.2)

1. BOARD_FLASH  0x0 ~ 0x800000 : LPC546xx_SPIFI_SFDP.cfx

*  Sugger debuger download up to 512k Limit

    A) Normal operation within 512k image size : OK

    B) Image size over 512K is a download error : 512k download limit

2. Please tell me the solution config

2 返答(返信)

1,379件の閲覧回数
karthikjai
Contributor II

how to display an image in lpc54628

can you help me by providing a program.

0 件の賞賛
返信

1,388件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Jongsub

This is the source code of the LPC546xx_SPIFI_SFDP.cfx, pls check the code and try to modify it so that it can adapt to the 1M limit.

C:\nxp\MCUXpressoIDE_11.1.1_3241\ide\Examples\Flashdrivers\NXP

BR

XiangJun Rong

 

0 件の賞賛
返信