MCUXpresso LPC54102 dual core project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso LPC54102 dual core project

跳至解决方案
4,568 次查看
eu_mtaverna
Contributor III

Hi all,

I just created a LPC54102 dual core project in MCUpresso following the guide. (Core M4 = Master, Core M0 = Slave).

After that I want to confiugre the LPC peripherals by MCUXpresso Config Tools but it works only on Master M4 core. When I try to open MCUXpresso Config Tools relative to the Slave core an error message appears :

"The project does not contains any configuration/source file to import open configuration. Open configuration failed due to unknown reason".

What about this issue? I noted that no .mex file appears on Slave project.

What is the correct way to configure the Slave peripherals by MCUXpresso Config Tools?

Thanks.

 

0 项奖励
回复
1 解答
4,530 次查看
eu_mtaverna
Contributor III

Thanks for replay,

I think I will configure peripherals manually.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,535 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

Do you use standalone MCUXpresso configure tool or integrated in MCUXpresso IDE?

I test with MCUXpresso IDE V11.6, it can work well:

Alice_Yang_0-1663901378666.png

 

BR

Alice

 

 

0 项奖励
回复
4,521 次查看
DanielR
Contributor I

I am curious Alice is the example you are showing a dual core project?

Daniel

0 项奖励
回复
4,508 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Yes, this is a dual core project under SDK demo:

Alice_Yang_1-1664162986137.png

 

BR

Alice

 

0 项奖励
回复
4,531 次查看
eu_mtaverna
Contributor III

Hi,

I'm working with integrated MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

0 项奖励
回复
4,560 次查看
DanielR
Contributor I

I saw the same issue. Unfortunately I don't have a great solution. I ended up working with a combination of two solutions:

1) Configure the peripheral under the M4 project and then manually copy the configuration code over to the M0+ project.

2) Abandon the MCUXpresso Config Tool for peripherals. It works well for pin assignments and configuring the clocks, but beyond that I found it to be very limiting. I had better results writing the config myself after reading the API Manual and the LPC5410x User manual (UM10850).

0 项奖励
回复
4,531 次查看
eu_mtaverna
Contributor III

Thanks for replay,

I think I will configure peripherals manually.

0 项奖励
回复