MCUXpresso IDE vs Config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE vs Config

1,276 Views
JK_265
Contributor III

I have to say I am a little confused about the MCUXpresso IDE and Config tools.

The IDE will not let me select IAR as the toolchain, so the auto-generated code contains the 'portable' code for GCC.  I manually have to copy a few .C modules and a .ICF file from an IAR-specific example project.

On the other hand, the Config tool allows me to configure the toolchain to IAR, but does not allow SDK management activities.  So the auto-generated code from the Config tool does not include any components/drivers, etc...  Again, this would result in me manually copying files into my project.

Am I confused or is it not currently possible to auto-generate everything?  If not, are there plans to remedy this?

Thanks!

 

0 Kudos
Reply
1 Reply

1,260 Views
Alice_Yang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply