MCPWM driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCPWM driver

867 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by swiebertje on Tue Nov 25 07:03:19 MST 2014
Hi there,

We're migrating our custom LPC4357 board support package from CMSIS to LPCOPEN. In CMSIS there was a Motor Control PWM driver which is missing from LPCOPEN (2.12). I noticed that the SCT is now used for generating a PWM. Our board is wired to use P4_0 as a PWM output pin but this pin is not configurable to be used as a SCT output.

For now I think the only way to overcome this is to keep using the CMSIS MCPWM driver?
I was wondering if MCPWM will be supported by LPCOPEN in the future?

Regards.
Labels (1)
0 Kudos
Reply
0 Replies