MCPWM driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCPWM driver

872件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by swiebertje on Tue Nov 25 07:03:19 MST 2014
Hi there,

We're migrating our custom LPC4357 board support package from CMSIS to LPCOPEN. In CMSIS there was a Motor Control PWM driver which is missing from LPCOPEN (2.12). I noticed that the SCT is now used for generating a PWM. Our board is wired to use P4_0 as a PWM output pin but this pin is not configurable to be used as a SCT output.

For now I think the only way to overcome this is to keep using the CMSIS MCPWM driver?
I was wondering if MCPWM will be supported by LPCOPEN in the future?

Regards.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)