MCB4350 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCB4350 BSP

1,342件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Thu Jan 08 12:58:48 MST 2015
I have the development board MCB4350 from Keil. I'd like to test some graphics functionalities with emWin, but the only BSP available is for MCB1700 (a similar board).

Is the BSP for MCB4350 available, or should I port the MCB1700 BSP? Did someone make the same port in the past and would like to share the result?
ラベル(1)
0 件の賞賛
返信
1 返信

1,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Jan 08 13:16:31 MST 2015
Hi giusloq,
Below example uses emwin library on MCB4300 board. You can take it an example for your development
http://www.lpcware.com/content/project/lpc4300-internet-radio-demo/download

0 件の賞賛
返信