MCB4300 blinky binary image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCB4300 blinky binary image

1,661 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sat Feb 08 06:06:25 MST 2014
Dear members,

I'm new to LPC4300. I'm using LPC21, LPC17, LPC11, LPC8 already. But right now I'm not yet fit enough to create even a simple blinky program for a LPC4300, because I don't have a development environment set up.
I'm still at the step of updating my flash programmer to support LPC4300, and this is a major update, because of the flash bank challange. So I need an absolutely reliable binary that I can use for testing, that easily shows some activity (like for example LED flashing) on this board?

Would anyone of you be so kind to provide me with one (*.bin, *.hex)?
I have a Keil MCB4300 with that row of 8 LEDs (P0.10..P0.14, P9.0..P9.2) below the LCD.
In return, I would provide my Linux flash utility  ;-)

Thanks in advance!

By the way, who is using Linux for programming the LPC4300 and who isn't even using an IDE?
What tools do you use for flashing it?
标签 (1)
0 项奖励
回复
3 回复数

1,619 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Mon Apr 28 18:25:11 MST 2014
It took some time and considerable effort to keep my promise. Here it is:

mxli-3.0
0 项奖励
回复

1,619 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sat Feb 08 09:52:05 MST 2014
Wow! Thanks a lot, Alex!

It works! Some Knight-Rider-style of a running light  :)

At first, I forgot to set active bank to A (didn't know it's necessary), but now it's working.
0 项奖励
回复

1,620 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abb on Sat Feb 08 09:14:18 MST 2014
Hello Marc,

I've built two HEX files from C:\Keil\ARM\Boards\Keil\MCB4300\Blinky project with UV4 for you. LPC4357-Flash-A-Blinky_FlashA.hex works on my Keil MCB4357 board.

Best regards,
Alex
0 项奖励
回复