LwIP RAM start address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LwIP RAM start address

1,430 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MaxOnCodeRed on Wed Nov 19 07:15:04 MST 2014
Hi,

I'm using LpcExpresso 7.4.0 and lpcopen_2_10_lpcxpresso_ea_devkit_4088.zip.
Inside projects that use LwIP (lwip_tcpecho_sa for example), the "data" starting address is 0x20000000 (RamPeriph32). If I run these projects, all work correctly.
If I try to set them to 0x10000000 (RamLoc64), the LwIP doesn't work.
Why?
If LwIP requires to have RamPeriph32, how is it possible to use the RamLoc64 also ?

Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,387 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MaxOnCodeRed on Mon Nov 24 00:51:54 MST 2014
Hi,

the board is our board previosly developed for ARM7 LPC2387 microprocessor and now we are testing it with LPC4078FBD100 that is a pin to pin replacement..

Thanks
0 Kudos
Reply

1,387 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Nov 21 13:42:02 MST 2014
Hi MaxonCodeRed,
Can you let us know which board and which LPC device are you using?
0 Kudos
Reply