LpcXpresso board broken

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LpcXpresso board broken

2,068 Views
dimitrissideris
Contributor III

Hi,

It is the second board (LpcXpresso 4367) that i bought (the previous one had a problem with uart pins and suddenly didn't print out to console.)

The new one when is powered on a green led is slightly dimmed up and when i try to debug, connection to linkserver is ok but then it appers that 0 available JTAG devices detected.

Also i cannot erase chip.

The most important thing is that when the board is powered on it is heating up very quickly.

Please i need some help.

Cannot afford for a third board.

Thanks in advance.

[EDIT]

i followed instructions from here Failed on connect: Ee(XX). Could not connect to core. | www.LPCware.com 

and the result of gdb trace is:

140,033 2-target-disconnect
140,034 3-gdb-exit
140,043 2^error,msg="You can't do that when your target is `None'"
140,043 (gdb)
140,043 3^exit

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

1,838 Views
sebastienboivin
Contributor I

I have the same problem with one of my board, the USB port even said over power. 

0 Kudos
Reply

1,838 Views
brendonslade
NXP TechSupport
NXP TechSupport

Hi Dimitiris,

we have contacted you directly by email about your board ... please check your email and follow up with us directly from there.

0 Kudos
Reply