LpcXpresso board broken

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LpcXpresso board broken

2,095 次查看
dimitrissideris
Contributor III

Hi,

It is the second board (LpcXpresso 4367) that i bought (the previous one had a problem with uart pins and suddenly didn't print out to console.)

The new one when is powered on a green led is slightly dimmed up and when i try to debug, connection to linkserver is ok but then it appers that 0 available JTAG devices detected.

Also i cannot erase chip.

The most important thing is that when the board is powered on it is heating up very quickly.

Please i need some help.

Cannot afford for a third board.

Thanks in advance.

[EDIT]

i followed instructions from here Failed on connect: Ee(XX). Could not connect to core. | www.LPCware.com 

and the result of gdb trace is:

140,033 2-target-disconnect
140,034 3-gdb-exit
140,043 2^error,msg="You can't do that when your target is `None'"
140,043 (gdb)
140,043 3^exit

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,865 次查看
sebastienboivin
Contributor I

I have the same problem with one of my board, the USB port even said over power. 

0 项奖励
回复

1,865 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Dimitiris,

we have contacted you directly by email about your board ... please check your email and follow up with us directly from there.

0 项奖励
回复