Lpc1788 onchip flash program load

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc1788 onchip flash program load

1,053 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by padmaja on Mon Jan 25 08:53:19 MST 2016
Hi,
I am working on uezgui-1788-70wvm module. I am using segger  j- link jtag for debug purpose. Ide is rowley cross works. If i download *.elf file to lpc1788 and debugging was ok. But when i power off and again on,nothing was comming. Means there is no program was stored in flash.If i want to load the program to flash which steps should i have to follow?
Thanks & regards,
Padmaja m.
Labels (1)
0 Kudos
Reply
1 Reply

1,017 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by padmaja on Wed Feb 03 00:35:05 MST 2016
hi,

problem solved by defining STARTUP_FROM_RESET at preprosessor properties of rowley cross works

thans & regards,
padmaja.
0 Kudos
Reply