Lpc 1788 going to reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc 1788 going to reset

675件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nil on Fri May 22 22:35:49 MST 2015


Hi,

                    I am using lpcopen_2_10_keil_iar_ea_devkit_1788 free rtos code for communicating via tcip.In this project IRAM1 is selected from 0x20000000 with size 0x8000(32k).I implement the heap_4.c. in SRAM at  address 0x10000000 with 50K size.My code is working well for some time (5-10min) but after that code stop executing some times i am getting error pbuf_free: p->ref > 0:650 in file ..\..\..\..\..\..\software\lwip\lwip\src\core.If anyone know about this error let me know.

thanks and regards
Nilesh
ラベル(1)
0 件の賞賛
返信
0 返答(返信)