Low-cost LPC1788 eval board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low-cost LPC1788 eval board

987 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Vladimir Khusainov on Wed May 30 05:38:06 MST 2012
Emcraft Systems has started shipping a low-cost ($99) LPC1788 eval board (LPC-LNX-EVB) immediatelly ready for U-Boot and uClinux. This is a USB-powered, 90mm x 100mm eval board that has on it an LPC1788 MCU, 32MB SDRAM, 16MB NOR Flash, an Ethernet interface and a number of expansion interfaces.

The board comes pre-loaded with U-Boot and uClinux.

Included with the eval kit is the Linux LPC1788 software distribution that supports both the Emcraft's LPC-LNX-EVB board and the Embedded Artists LPC1788-DEV-KIT board.

Further details can be found here:

http://www.emcraft.com/index.php/products/137
Labels (1)
0 Kudos
Reply
0 Replies