LoraWAN node library suggestions to connect to Things Network Gateway, SX1262 & LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LoraWAN node library suggestions to connect to Things Network Gateway, SX1262 & LPC55S69

ソリューションへジャンプ
3,652件の閲覧回数
gertvb
Contributor III

Hallo Everyone!

I am busy adding an SX1262 (Lambda62-8 module from RFSolutions) to an LPC55S69 with the aim of getting comms through to a "Things Network" Gateway

Can you please suggest a software library that I can use to create the node with? That handles all the stuff required to speak to a TTN Gateway like OTAA etc etc

There are just zillions of libraries on the net, from Semtech, from Lora Alliance, from IBM, from The Things Network and I am unsure which will be the easiest to integrate into an MCUXpresso project

Dankie!

A TechExplorer working with Embedded Software and Electronics in Agriculture and Alternative Energy
タグ(1)
0 件の賞賛
返信
1 解決策
3,463件の閲覧回数
gertvb
Contributor III

Hallo everyone,

Erich Styger did a nice project based on work done by Diego Bienz

https://mcuoneclipse.com/2021/12/30/lorawan-with-nxp-lpc55s16-and-arm-cortex-m33/

Kind regards

A TechExplorer working with Embedded Software and Electronics in Agriculture and Alternative Energy

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,464件の閲覧回数
gertvb
Contributor III

Hallo everyone,

Erich Styger did a nice project based on work done by Diego Bienz

https://mcuoneclipse.com/2021/12/30/lorawan-with-nxp-lpc55s16-and-arm-cortex-m33/

Kind regards

A TechExplorer working with Embedded Software and Electronics in Agriculture and Alternative Energy
0 件の賞賛
返信
3,639件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

We don't have an existing LPC55S69 LoraWAN node lib already ported. 

User has to port it by self. This site includes many useful resource, Hope this can help you.

https://os.mbed.com/docs/mbed-os/v6.10/apis/lora-tech.html

This is a reference design

https://www.nxp.com.cn/docs/en/nxp/application-notes/AN12257.pdf

 

Have a nice day

Jun Zhang