Looking for an efficient way to sample a digital signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for an efficient way to sample a digital signal

1,223件の閲覧回数
christian_oster
Contributor I

Hello,

i would like to sample a digital signal (HIGH / LOW) with a sampling rate of >=250kHz. Polling the data using a periodic timer interrupt seems like an inefficient way.

Can you recommend me a hardware component to sample digital data ? Maybe the SSP-Unit can be used for this ?

Thanks.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,135件の閲覧回数
chrispflieger
Contributor IV

You could use the SSP if you ran it in master mode with the pin tied to MISO, but you'd have to make sure it would run without any gaps between data. However, I would consider this method unreliable.

Otherwise, timer capture is the way to go.

0 件の賞賛
返信

1,135件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport


Hi Christian Ostermeier,

   Do you want to sample the digital signal's frequency? If yes, you can use the Timer module, the capture function.

   If you don't want to capture the frequency, please tell me the detail function you want to realize.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信