Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

1,829件の閲覧回数
andyjackson
Contributor III

Looking through the LPC5461x MCUXpresso 2.2 SDK there appear to be a number of full speed USB ROM device examples (using USB0), but none for using the high speed ROM device (using USB1).

Where can I find such examples, particularly for a VCOM device?

Thanks,

Andy

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,535件の閲覧回数
soledad
NXP Employee
NXP Employee

HI,

At this moment, we only have the LPC5461x MCUXpresso 2.2 SDK examples.

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,535件の閲覧回数
andyjackson
Contributor III

Hello Soledad,

Thank you for your reply. Is there any plan for a ROM based example in the near future? I have the full-speed (USB0) working, but our product plans require high-speed USB.

Thanks for your help,

Andy

0 件の賞賛
返信