Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

1,821 次查看
andyjackson
Contributor III

Looking through the LPC5461x MCUXpresso 2.2 SDK there appear to be a number of full speed USB ROM device examples (using USB0), but none for using the high speed ROM device (using USB1).

Where can I find such examples, particularly for a VCOM device?

Thanks,

Andy

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,527 次查看
soledad
NXP Employee
NXP Employee

HI,

At this moment, we only have the LPC5461x MCUXpresso 2.2 SDK examples.

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,527 次查看
andyjackson
Contributor III

Hello Soledad,

Thank you for your reply. Is there any plan for a ROM based example in the near future? I have the full-speed (USB0) working, but our product plans require high-speed USB.

Thanks for your help,

Andy

0 项奖励
回复