Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for a LPC5461x MCUXpresso SDK high speed USB ROM device example

1,844 Views
andyjackson
Contributor III

Looking through the LPC5461x MCUXpresso 2.2 SDK there appear to be a number of full speed USB ROM device examples (using USB0), but none for using the high speed ROM device (using USB1).

Where can I find such examples, particularly for a VCOM device?

Thanks,

Andy

Labels (2)
0 Kudos
Reply
2 Replies

1,550 Views
soledad
NXP Employee
NXP Employee

HI,

At this moment, we only have the LPC5461x MCUXpresso 2.2 SDK examples.

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,550 Views
andyjackson
Contributor III

Hello Soledad,

Thank you for your reply. Is there any plan for a ROM based example in the near future? I have the full-speed (USB0) working, but our product plans require high-speed USB.

Thanks for your help,

Andy

0 Kudos
Reply